AnsweredAssumed Answered

help need with 8510b now in demonstration mode

Question asked by i5uxj on Oct 16, 2007
Latest reply on Jan 1, 2009 by SatAntGuy
After load Cal Kit data  tape , the instrument was in error , the gpib data address was wrote with bad address (example 2467) , after correct all gpib address , reset with test button , the 8510b work , but is impossible to calibrate or load or save because answer
ERROR:DEMONSTRATION TIME ELAPSED , then the instrument is unusable until the reset , is there some location of memory were i can write the correct value with poke command ?
i do not have the firmware tapes .
Hello Alfredo

Outcomes