Dear Sir,
I need to generate two layers layout using ADS2009. Can you anybody help me to generate the two layers as shown in the below in the figure TWO_LAYER_LAYOUT_EXAMPLE. What are the setting need to do for generating two layers from schematic to layout generation . We need upper layer and bottom layer , in between upper and bottom layer , there is substrate gap, how to set this height of the substrate between two layers. I need to generate as shown in the figure TWO_LAYER_LAYOUT_EXAMPLE. What I need to connect in the schematic of the ADS to generate as shown below. Can you anybody having help document for generating two layers in ADS 2009 , can you show me.
I need to generate two layers layout using ADS2009. Can you anybody help me to generate the two layers as shown in the below in the figure TWO_LAYER_LAYOUT_EXAMPLE. What are the setting need to do for generating two layers from schematic to layout generation . We need upper layer and bottom layer , in between upper and bottom layer , there is substrate gap, how to set this height of the substrate between two layers. I need to generate as shown in the figure TWO_LAYER_LAYOUT_EXAMPLE. What I need to connect in the schematic of the ADS to generate as shown below. Can you anybody having help document for generating two layers in ADS 2009 , can you show me.
The thickness of the substare is set by the substrate instance shown on your schematic.