AnsweredAssumed Answered

SCPI Command for Output Voltage not Sense'd voltage

Question asked by drdroege Employee on Feb 19, 2014
Latest reply on Jul 30, 2019 by jasonliu2426
Hi,

I'm using two modules (N6762A & N6784A) in an N6700B mainframe.  I know the command to query the normal (set or programmed) output voltage but am looking for a command to query the actual output voltage at the power supply terminals. When used in remote sense, the power supply output will be a little larger than the programmed voltage to compensate for path loss to the load - is there a query command to retrieve that larger voltage?  Also, is the value retrieved a calibrated voltage measurement?

Thanks,
David  

Outcomes