AnsweredAssumed Answered

SCPI commands

Question asked by huskerli on Aug 28, 2013
Latest reply on Sep 10, 2013 by lhornburg
Hello all,

I have two questions want to ask here:

1. How can I check the SCPI commands I wrote is right or not, where can I run it?

2. I want to use PULSE to do some measurement,but I just found out this SCPI command I am using

    :SOURce[1]:FUNCtion:SHAPe" is not supported by the instrument which is Agilent B2901A 

    I get the command from the Agilent B2900 Series SCPI command reference page 325.

    I just do not get it since the instrument has that functionality and I been manually tested successfully why there is no SCPI command for that?

Thanks

Outcomes