Hi!
With the Toolkit I load signal from the .mat file in generator. A recorded signal is continuous. After pressing play in toolkit on the spectrum analyzer, signal periodically disappears.There is a pause between the repeat play copy record? How to get rid of it? signal has a length of 76800 samples * 12.
Edited by: dimazz on Oct 5, 2013 12:50 AM
With the Toolkit I load signal from the .mat file in generator. A recorded signal is continuous. After pressing play in toolkit on the spectrum analyzer, signal periodically disappears.There is a pause between the repeat play copy record? How to get rid of it? signal has a length of 76800 samples * 12.
Edited by: dimazz on Oct 5, 2013 12:50 AM
Two things come to mind immediately:
1) Make sure that the behavior is not part of the waveform design.
2) Make sure that the ‘ENDIANess’ (Big or Little) is correct.
Or Else
If we can get either the Matlab ‘.m’ file or the actual waveform file ‘.mat’, we can then set this up and investigate further.
Hope this helped -
I paste the data file what i use. can you check this?
Attachments
I have used your .mat file to download the waveform but I am not able to see any problems. The waveform played out continuously as expected.
Please ensure that the N5182A trigger type is set to continuous free run.
Regards -
yes, i checked trigger type, set continuous (free run).
perhaps disappearance of the spectrum due to some failures in our apparatus =(
anyway thanks for the help and tenderness.