AnsweredAssumed Answered

HP4155A error code

Question asked by jackos32 on Jun 19, 2014
Latest reply on Jun 24, 2014 by ELSES

Hello

I got a problem when I used a HP4155A to do some DC sweep measurement.

I set up 2 voltage inputs with sweep-order 1 & 2 ,and 1 voltage input as constant in my ic-cap setups.

But when I started measurement ,the 4155A didn't set 2 SMUs as VAR1/VAR2 and an error code popped up

" ERROR 180 : illegal setup , target module is not installed"

My previous version of ic-cap is 2006B and I never had this problem with the same instrument.

Any suggestion will be appreciated, thank you.

Outcomes