AnsweredAssumed Answered

Synchronize Receiver to Pulse Generator in N5242A Programmatically

Question asked by ranjan on Sep 19, 2013
Latest reply on Sep 25, 2013 by Dr_joel
Hi,

    I am facing problem regarding receiver synchronization while doing pulse generation in remote mode (using SCPI commands). It is working in Wideband detection mode if i use pulse generation in Local Mode. It is not working in wideband mode when remote mode is used. It is automatically set to narrowband when commands are used programmatically. I am attaching five snapshots for local and remote mode operation.

1. *PulseGeneration_LocalMode.png* : It is operated in Local Mode. Here IFBW is set to 150 KHz automatically. I have selected wideband mode in *Autoselect Pulse Detection Method*. 

2. *ReceiverSynchronization_LocalMode.png* : Pulse0 Delay is automatically set in *Synchronize Receiver to Pulse Generator pulse0*. Internal trigger is selected in *Pulse Sync Trigger*.

3. *PulseGeneration_RemoteMode.png* : I used SCPI Commands to generate pulse programmatically, but here IFBW was set to 100KHz. I have used command to set IFBW as 150 KHz (refer point 1). After setting IFBW to 150 KHz i am getting same values as per  *PulseGeneration_LocalMode.png*.

4. *ReceiverSynchronization_RemoteMode.png* : Pulse0 Delay is showing 0 psec in *Synchronize Receiver to Pulse Generator pulse0*. I am using SCPI command to set source as internal in  *Pulse Sync Trigger*. *I am not getting any command to set Pulse0  Delay for receiver synchronization*.

5. *PulseGeneration_RemoteMode_Narrowband.png* : Here i have used SCPI command to select *Autoselect Pulse Detection Method*, but it is working in Narrowband mode. It was working in Wideband mode (refer point 1) when Local mode is used.

     Kindly help me to find solutions for this problem.

Best Regards,
Ranjan  

Outcomes