HI AND THANKS FOR HOSPITALITY, I HAVE THE SAME PROBLEM ON MY HP 8563E and HP8714B
keyboard: in the both units when the machines are COLD as external temperature.. a part of the keyboards are not responding, if i use a hot fan after some minuts all is OK, in yje hot season also Ok. i think that is for a great use of the kb, any ideas ??? Thanks Bobby I1RRT
keyboard: in the both units when the machines are COLD as external temperature.. a part of the keyboards are not responding, if i use a hot fan after some minuts all is OK, in yje hot season also Ok. i think that is for a great use of the kb, any ideas ??? Thanks Bobby I1RRT