This is regarding the ground reference for the internal and EDge ports in ADS momentum (Version used ADS2012 08).
Going through the following link and other documentation, would like to make sure that I am doing it correct.
http://muehlhaus.com/support/ads-application-notes/em_line_ground
Attached below are the substrate definition and layout==>
Read that the Edge port P1 and internal ports P4 P7 etc. will get implicit ground reference if there is "Infinite ground plane in the substrate definition"
How to do this in the substrate definition ?.
Is my substrate definition OK and take care of the infinite ground plane?
Do I need to select the option "Add Reference pin " in my case?
Also, in my PCB, I have shielding around 1 cm above the copper. I have defined it as cover in the substrate definition. Am I doing it correct?
From your picture, I do not understand what P1 represents? You have another thread open where that P1 is large, along the entire edge. What you do you want to model with such a wide port?