AnsweredAssumed Answered

82350B PCI GPIB board: which resources it uses?

Question asked by rodolfogiovanninetti on Jul 23, 2014
I am testing a 82350B board in a HP Compaq Pro 6300 Microtower PC (model code QV983AV) with Windows 8.1 64 Pro. I installed the IO Libraries Version 16.3.17914.4 and then I installed the board. In the device manager, the board is identified with the correct name, but it is marked with a yellow triangle with an exclamation mark. The error says "This device cannot find enough free resources that it can use". What are the resource that the board needs? How can I find out how to fix this issue? If I have a listing of resources that it needs (I believe that they are at least I/O ports, IRQ, Memory) I can check where they are used and by which device.


Thank You and regards

Rodolfo Giovanninetti

Edited by: Rodolfo Giovanninetti on Jul 23, 2014 10:56 AM  

Outcomes