AnsweredAssumed Answered

GPIB/SCPI- CALC Command Works Occasionally

Question asked by anguilin on Jun 21, 2013
Latest reply on Jun 21, 2013 by anguilin
I currently have different programs for 2 other instruments which work very well.

For some reason this command works spontaneously:

CALC:MARK1:FUNC:EXEC MIN

The error message text is:

"The SCPI command received has caused error number 103: "CALC measurement selection is set to none"

I'm guessing there is a reset or reboot condition which defaults the marker to MARK1 but if I don't set it, this is when I see it.

I checked the marker ID by using 
CALC:PAR:CAT? 

But I'm not sure if that's the correct query.

Any help is appreciated.  

Outcomes