AnsweredAssumed Answered

Looking to buy a GPIB upgrade card for a HP8594e spectrum analyser

Question asked by joemcc on Sep 9, 2013
I have a HP8594e analyzer with option 23 fitted (the serial interface). I want to upgrade to GPIB. Does anyone have this option board they are willing to sell? My unit has a serial number prefix < 3523A so needs the board p/n 5062-6454 which as far as I know has only the GPIB connecter fitted. I'm not sure if the option 41 dual interface card (p/n 08590-60380) can be fitted to this model. The info here http://www.home.agilent.com/agilent/editorial.jspx?cc=IE&lc=eng&ckey=1000001916:epsg:faq&nid=-11143.0.00&id=1000001916:epsg:faq seems to indicate that it could be fitted at the factory once upon a time.

Thanks,

Joe

Edited by: Joe McC on Sep 9, 2013 2:33 PM  

Outcomes