How do you change trace and limit color or better presentation.
e.g. I want trace-1 to be dk. green and limit lines in red. Further, the limit lines should be thicker. How do i do it?.
e.g. I want trace-1 to be dk. green and limit lines in red. Further, the limit lines should be thicker. How do i do it?.
The colors of the traces cannot be changed. There are 3 different traces that you can use in the EMI Receiver mode, all with a different color, so you could use the trace that has a color that you would prefer. The colors of the limit lines change to match the color of the traces that you are comparing them to, and there is no way to change the thickness of the lines.
Mike