Hello. My company just buy the new IC-CAP 2013.01.
When I am trying to use ADS simulator in IC-CAP environment , simulation debugger shown messages as below
---------------------------------------------------------------------------------------------
"Error detected by hpeesofsim during circuit set up `dc1'.
An appropriate license for linear features is not available. This
feature must be license before it can be used.
FlexLM error message:
License server system does not support this feature.
Feature: iccap_analysis
License path: *****@*******.******.com
FLEXnet Licensing error:-18,14
---------------------------------------------------------------------------------------------I
It looks like that I could not call ADS simulator if my ADS in PC uses license server.
Is there any solution to solve it if I don't have a fixed license file?
Thank you
When I am trying to use ADS simulator in IC-CAP environment , simulation debugger shown messages as below
---------------------------------------------------------------------------------------------
"Error detected by hpeesofsim during circuit set up `dc1'.
An appropriate license for linear features is not available. This
feature must be license before it can be used.
FlexLM error message:
License server system does not support this feature.
Feature: iccap_analysis
License path: *****@*******.******.com
FLEXnet Licensing error:-18,14
---------------------------------------------------------------------------------------------I
It looks like that I could not call ADS simulator if my ADS in PC uses license server.
Is there any solution to solve it if I don't have a fixed license file?
Thank you
With proper licensing, one can link IC-CAP to ADS. It sounds like there is a problem with the licenses that you have
received/configured. I suggest to email eesof_support@agilent.com and cc me, and we will make sure the issue is resolved..
On Windows, make sure you have defined ADS_DIR in the environment variables, to point to the ADS installation directory,
and on Linux, make sure to define HPEESOF_DIR to point to the ADS installation directory.
I would also recommend, that for newer versions of IC-CAP, like ICCAP 2013.01, to also use newer versions of ADS, eg.
ADS 2012 or ADS 2013. (If one tries to run a new version of one product with an old version of another, this can create
licensing setup incompatibities)..
Please contact us: eesof_support@agilent.com and cc me: else_schmidt@agilent.com and we will be glad to assist further.
Best regards
Else