hi,
On the E8257D can we do a logarithmic step for frequency sweep? If so how do we do it? One way is to compute the frequency points that occur when doing a log sweep and enter them in the list sweep. This is a cumbersome process.Can we do it directly?
Rgds
On the E8257D can we do a logarithmic step for frequency sweep? If so how do we do it? One way is to compute the frequency points that occur when doing a log sweep and enter them in the list sweep. This is a cumbersome process.Can we do it directly?
Rgds
To set log step sweep, do the following setting on the instrument under the Sweep/List tab.
Press: Sweep/List->Sweep Type->Step
Under Configure Ramp/Step sweep->more->Step Spacing->Log
See attached.
Regards -