Sir,
I have connected the one transistor is feedback to the other. How to achieve the biasing for two transistors Vds = 3V and Ids=60mA.
I have used the two ATF54143 transistors, and achieved the biasing at one transistor X2(shown in figure) Vds=3v (potential difference of 3 volts and Ids = 60mA). But I couldn't achieve the difference of voltage of 3 volts at X1 transistor (shown in figure) at Vds and Ids =60 mA. I have connected the active feed back of connection transistor as I followed the example of Active_Feed_Example(it is shown in the figure). Can you anybody help me to achieve the Vds=3Volts and Ids=60mA at the two transistors.
I have connected the one transistor is feedback to the other. How to achieve the biasing for two transistors Vds = 3V and Ids=60mA.
I have used the two ATF54143 transistors, and achieved the biasing at one transistor X2(shown in figure) Vds=3v (potential difference of 3 volts and Ids = 60mA). But I couldn't achieve the difference of voltage of 3 volts at X1 transistor (shown in figure) at Vds and Ids =60 mA. I have connected the active feed back of connection transistor as I followed the example of Active_Feed_Example(it is shown in the figure). Can you anybody help me to achieve the Vds=3Volts and Ids=60mA at the two transistors.
Thank for your help, I added Ic2. Now I am achieving the Ids=60 mA at the both transistors. But I am not getting the voltage difference of Vds= 3volts at the X1 , but I am getting the voltage difference of 3 Volts and Ids=60mA at X2. How to achieve the voltage difference of Vds=3V at X1.
Attachments
Some one can help me to resolve this difficulty
The ADS Discussion Forum is a community created to allow you to communicate directly with other ADS users around the world and is designed to be a place to ask and answer other users’ questions, exchange ideas, and share tips and tricks for using ADS.
The ADS Discussion Forum is not the best or primary means to contact Agilent EEsof Technical Support.
To get help with your issue, I suggest you contact Agilent EEsof support directly or access ADS Support and Documentation by visiting ADS Support Home http://edocs.soco.agilent.com/display/support/ADS+Support+Home.
Joe Civello
ADS Product Manager