AnsweredAssumed Answered

Problems with Remote controlling of E5061B using labview

Question asked by orok on Sep 18, 2013
Latest reply on Sep 23, 2013 by takeshio
Hi,

We are developing a labview application (LV2011) for remote controlling E5061B.
We also use the available ENA series instrument drivers.

Normally the application functions as intended, but the problem start when E5061B detects an internal error.

The intended test progress is to start a sweep. If the instrument detect an error, we want to abort the sweep and start a new sweep with a corrected setup.

The problem is that the instrument seems to be communicationally blocked when it have internal error(s) detected, it not responding normaly.


Is there any "master reset" command that we could use?


I will be happy if anyone could give me som advise to solve the problem? 


regards
Oddgeir  

Outcomes