AnsweredAssumed Answered

N5222 PNA Launch Cal Wizard Issues

Question asked by uke on Feb 4, 2014
Latest reply on Feb 5, 2014 by johanericsson
I am trying to write a small driver for the PNA and one of the requirements is to launch the Cal Wizard from software. However when I use the command (as indicated in the PNA help pages) SYSTem:CORRection:WIZard MAIN I receive the error: "The SCPI command received has caused error number -113 “undefined header”". I normally seem to get this error when a command is not recognised.
 
After digging around in the forums etc I found the suggestion that it may be that four rather than three of the letters that are capitalised in the "wizard". However I was met with the same error upon trying this.
 
My assumption is that I need to be calling something prior to launching the cal wizard, but what that may be I dont know. I already have code in place which selects a measurement to make the appropriate channel active etc, using CALCulate:PARameter:SELect.
 
If anyone could shed some light on this it would be much appreciate  

Outcomes