AnsweredAssumed Answered

Measure clock jitter with MSO-X 4104A

Question asked by pollarbear on Nov 21, 2013
Latest reply on Nov 22, 2013 by algoss
Hi experts,

I am debugging USB3.0 interface, my FPGA outputs a signal of LVCMOSS, and this signal is just connect to a test point, the trace impedance is 50ohm.

I got a result below. The bandwidth of my probe is 1GHz, I have several questions about it.

a) Why the low level is about 1.7V, not 0V?

b) Why does the falling edge look so bad? 

Any comment is welcomed.

Thanks.
Chris.  

Attachments

Outcomes