AnsweredAssumed Answered

discrete step size optimization variables?

Question asked by robertem2k on Mar 17, 2014
Latest reply on Apr 11, 2014 by wrivas
Is it possible in Genesys to run optimization using discrete step size variables (instead of continuous variables, with only min and max limitations)?

I would like to test a given design sensitivity/limitation to practical quantized optimization variables.  

For example, if an attenuator is one of my optimization variable, I would like to see what are the optimization limitations if my variable attenuator can be only change in the steps of 0.5dB. Obviously I might have more than one of such discrete step variables in the optimization set.

Thank you and best regards,
Robert.  

Outcomes