would like to load a pre generated *mat, *.txt, *.bin, etc... waveform files to the M8190 via VBA. loading sequentially via vba to coordinate measurements with a scope. i have not programmed to a pxi or hslip or tcpip/socket and would appreciate any help. the example files that were included in the install of the m8190 are written in vb and i dont have a mapping between the "imports" files and the reference libraries in vba. many thanks