AnsweredAssumed Answered

Physical port set up restrictions

Question asked by Leyo on Mar 2, 2014
Latest reply on Mar 3, 2014 by volker_muehlhaus
Hi,

This is regarding the length of the copper edge on which an edge pin can be placed.
As per the attached ADS documentation, the length of the edge on which edge pin is located should be less than lamda/10.

In the attached layout the edge on which I am placing an edge port is 15 cm. lamda  of this set up is  10 12 cm and lamda/10 will be 1.2 cm. This violates the ADS physical port set up restrictions. Is my analysis correct?  

Attachments

Outcomes