AnsweredAssumed Answered

Can't annotate DC analysis

Question asked by jimmydean on Apr 25, 2014
I get the following Warning when attempting to Annotate DC solution: http://imgur.com/zr6UMzA

"Either dc analysis was not performed in the last analysis of the design or dc data of Swept analysis cannot be back-annotated at this time"

I can't seem to figure out what was done differently between two schematics I saved. One was saved at an earlier stage and nearly all the components are very similar. I have tried deleting the 'DC' component and various other things but it seems I can't get the annotation anymore. Any ideas?

Thanks in advance.

Solved: Something to do with the S Parameters component. Using different one yields DC annotations. Not sure why.

Edited by: jimmydean on Apr 25, 2014 2:49 AM  

Outcomes