AnsweredAssumed Answered

Data Link software reports "CalKitEditor.exe has stopped working"

Question asked by drkirkby on Nov 25, 2013
Latest reply on Nov 25, 2013 by drkirkby
I  no longer have a FieldFox (I used to own an N9923A), but I am are trying to create a calibration kit file for a custom SMA calibration kit, that someone can load into a FieldFox. I seem to be hitting a bug in the Data Link software, version 4.64. 

I used the standalone CalKitEditor Rev: 1.0.5018.0 (Sept 2013) 

http://na.tm.agilent.com/pna/apps/#calkiteditor

to create the attached .xkt file - note the extension is .xkt and not .xml, since CalKitEditor does not allow one to save a .xml file, but it does allow one to save a .xkt file which I believe should upload to the FieldFox via Data Link software. 

If I attempt to open that .xkt file in the Data Link software, version 4.64, it reports "CalKitEditor.exe has stopped working". But the same file opens in the standalone CalKitEditor Rev: 1.0.5018.0. 

The computer I am using is a Sony laptop, with 32-bit Vista Business Edition which has service pack 1 installed.  

Dave  

Attachments

Outcomes