Hello,
I have a custom C++ application that talks to an Agilent E4434B through VISA with GPIB. The application works well however we had to switch from using the E4434B to an E4438C. For the most part the change over was seamless. However, we have noticed off differences in behavior and every time I look into it, it seems that the SCSI commands are just a little bit different between the two instruments.
Two questions:
1) Should we upgrade all the SCSI commands to what is listed in the E4438C manual?
2) Does anyone know the what the SCSI differences are between these two generators?
Thank you
I have a custom C++ application that talks to an Agilent E4434B through VISA with GPIB. The application works well however we had to switch from using the E4434B to an E4438C. For the most part the change over was seamless. However, we have noticed off differences in behavior and every time I look into it, it seems that the SCSI commands are just a little bit different between the two instruments.
Two questions:
1) Should we upgrade all the SCSI commands to what is listed in the E4438C manual?
2) Does anyone know the what the SCSI differences are between these two generators?
Thank you
E4434B
:mem:data:pram:block #ABC
E4438C
:mem:data:pram:file:bloc "PRAM_DATA",#14Yq8L