AnsweredAssumed Answered

E8358A firmware question

Question asked by Dr_Bob on Mar 24, 2014
Latest reply on Mar 27, 2014 by jvall
Hi folks,

We have a couple of PNA analysers including an obsolete but still useful RF PNA E8358A. This has the 1.1GHz CPU and runs what I believe is the last official firmware release for this unit, A.07.50.67.

However since this runs the older firmware compared to the newer PNAs the look and feel of the interface is very different - trace labels on left, menu structure different etc. So, my question is this, can the E8358A run more up-to-date firmware which would give similar menu structure to the newer A.09.XX.XX versions?  

Outcomes