AnsweredAssumed Answered

Automated adjustments - HP9000 series software, any way of running in VEE?

Question asked by k_purden on Jun 3, 2013
Latest reply on Jun 7, 2013 by Mike
Hi I am relatively new to this but I have a 8562E analyser which is in need of a frequency response adjustment. This can be done manually, I know, but I found the software for it on the Agilent support pages (http://www.home.agilent.com/agilent/editorial.jspx?cc=GB&lc=eng&ckey=526335&nid=-536902966.536880938&id=526335) but the software for the adjustment I need is for an old HP9000.

My question being is there any way of running this on windows? I currently have access to various versions of VEE (mainly 5.01 on windows 95 and 8.01 on XP)

If it is in any way possible it would save me a lot of time as I also have a backlog of 8563Es which are in a similar state. I know one simple solution is to use the TAM module for some adjustments but here in the UK I am finding it exceedingly difficult to source one

Any help will be greatly appreciated

Thanks in advance

P.S if I have posted this in the wrong place, or if there is a thread already existing on this please point me in the right direction :)  

Outcomes