AnsweredAssumed Answered

N5230 VNA Questions

Question asked by rftech3000 on May 15, 2013
Latest reply on May 17, 2013 by daras
So im contemplating sending my old 8510C system into retirement and go for something newer and fancier, there seem to be bunches of N5230 VNA on the market right now but most of them are RF models to 6 or 9GHz , so my question is : does agilent offer any upgrade kits to change lets say a 6GHz into a 20GHz or a 20GHz into a 40GHz VNA ?  is this cost effective ? how do those VNA Compare to the 8510C in terms of accuracy ? the 8510C had a function to do a testport power calibration with a E4418B meter, does the 5230 offer a similar function ?  

Outcomes