AnsweredAssumed Answered

Can LabVIEW programmatically set N6702B to local after using it in remote?

Question asked by mark005 on Mar 14, 2014
Latest reply on Mar 21, 2014 by MattC
I see in the quick reference under SCPI commands (page 21) that there is a command that "specifies the Remote/Local state of the instrument."

I downloaded and installed the n6700 LabVIEW drivers but I can't find one that has this command. I need it because I need to return the power supply back to local when done using it in remote mode.


Do I have to write a LabVIEW vi for this or am I not seeing the vi in the LabVIEW N6700 series instrument drivers palate that already has this command?  

Outcomes