AnsweredAssumed Answered

Comaptibility TestExec and Vee

Question asked by Ever on Jan 9, 2014
Latest reply on Jan 24, 2014 by Ever
Hello,
which version of TestExec can be used with which version of VEE?
Is there somewhere a table with all versions of the two programs?

In my case it is: Currently i am using TestExec 4.1 and Vee 6.01
Can i update TestExec to 6.1.2 and still use Vee 6.01? Or do i also have to update the vee-version?


Thanks  

Outcomes