AnsweredAssumed Answered

burst bandwidth limited

Question asked by bmag on Nov 11, 2013
Latest reply on Nov 13, 2013 by lhornburg
I would like to generate a band limited burst (gausian tone burst) that looks like the attached file.  Is there a way to do this with a function generator?  I have a 33220A and a 33500B?  I need to run the function generator remotly via GPIB.  I need to change frequency so I don't think I can create a custom waveform for every possible frequency.  I can set the generator to AM modulation and get this signal but I not for a burst.  Any ideas?  I need the software trigger command to send a single burst.  

Attachments

Outcomes