AnsweredAssumed Answered

Using two Network analyzer, one as source and receiver

Question asked by stanleysg on Nov 10, 2013
Latest reply on Nov 19, 2013 by tominlyon
hi,

just wonder, if i am using two network analyzers,  one acting as a pure source, and another one acting as a pure receiver.

with same programming commands, and setting to absolute ratio, same number of points and other settings etc.

will this able to conduct the measurement successfully? so that i know source output, and receiver input result and doing the calculation myself.

both network analyzers will be connected through antenna for the signal tranmission and receiving.  

Outcomes