AnsweredAssumed Answered

E4413A Sensor backing up the EEPROM ?

Question asked by rftech3000 on May 15, 2013
Has somebody ever thought about creating a application to create a backup immage of the EEPROM for the E4413 , or maybe somebody already done so ?
what i was thinking is using the DIAG:DET:EEPR? command to read out the contents of the EEPROM and store them in a XML file , if the EEPROM goes bad you can just replace the bad one with a new blank one and re-store the file !
thoughts ?

Outcomes