I have two E4407Bs and 8565E which exhibit a unusual failure in measurements below 50 dB down from full scale. For example I am providing a 50 MHz 0 dBm, TB phase locked signal to the input. When the analyzer is in the default 10dB log mode,1 KHz span or lower, RBW/VBW auto and at 0 dBm reference I get the correct amplitude from FS to -96 dBc. However, when I put the unit into zero span at about -50 dBc I get a very unstable display which get worse as I try to decrease the signal. @ 300 Hz RBW, I have a 20 dB swing and @ 10 Hz RBW, I have a 3 dB swing. When I put the instruments to a 1 KHz RBW the instruments reads correctly and stable. The system F/W is A.14.00 and A.14.06. The 856xE series has 1999 F/W. All three do not have FADC option. I tried this test on a PSA and it works as one would expect all the way down to -98 dBc in all bandwidths. Is this an inherent H/W design problem for the earlier series. I have end user that is insisting the instrument is broken.
Thanks, Dave
Thanks, Dave