Hello MXG Users,
Where can I find information on the file format for an ARB file header?
Chp 5 of Programmers Guide, Table 5-7 offers the command: MMEM:DATA "HDR1:",.
Many pages are devoted to explaining byte swapping of the i/q samples and there is a page or so on the marker file..... But I have scanned Chp 5 for a description of what should be (and what can be) in the header file and it's associated syntax to no avail. The best I could do was find a code snippet on p 296 which yielded :sour:radio:arb:header:write ....... and I failed to find an entry in the manual for this command.
The documentation suggests that this is where all the hardware settings go - sample rate, scaling etc, which makes sense since I want these tied to the waveform.... Would just be nice if the programming manual told you the format....
Please help
thanks
andy
Where can I find information on the file format for an ARB file header?
Chp 5 of Programmers Guide, Table 5-7 offers the command: MMEM:DATA "HDR1:
Many pages are devoted to explaining byte swapping of the i/q samples and there is a page or so on the marker file..... But I have scanned Chp 5 for a description of what should be (and what can be) in the header file and it's associated syntax to no avail. The best I could do was find a code snippet on p 296 which yielded :sour:radio:arb:header:write ....... and I failed to find an entry in the manual for this command.
The documentation suggests that this is where all the hardware settings go - sample rate, scaling etc, which makes sense since I want these tied to the waveform.... Would just be nice if the programming manual told you the format....
Please help
thanks
andy
This information doesn’t exist. We will see what, if anything , can be done.
Regards -