AnsweredAssumed Answered

E4360 SAS transient section does not respond to some SCPI commands

Question asked by AlphaBob on May 14, 2013
Latest reply on May 15, 2013 by MattC
E4360 SAS Firmware vision A.01.07

After  programming a transient list, setting the trigger source and enabling the output 

The command INIT:TRAN (@1,2) is suppose to initiate the trigger subsystem

But it does not.

The command INIT:CONT 1, (@1,2) is suppose to put the trigger subsystem into continuous initiated mode

But it does not.

The command LIST:TERM:LAST 1, (@1)  is suppose to make the SAS stay at the last transient step at the end of the list.

But it does not.

All of these command are ignored by the E4360 SAS Firmware vision A.01.07.

Is the manual wrong or are these units buggy?

Edited by: AlphaBob on May 14, 2013 2:53 PM
Edited by: AlphaBob on May 14, 2013 2:53 PM  

Outcomes