AnsweredAssumed Answered

How to Enable Two or More Traces in Labview?

Question asked by themagicfarmer on Aug 1, 2013
Latest reply on Aug 1, 2013 by themagicfarmer
Hi there, my first post here :)

I'm trying to figure out a way to setup two traces in Labview for the N9010A EXA Signal Analyzer. 

It doesn't work by simply adding a "configure trace type.vi" in that channel. I also tried duplicate the whole thing one for each trace, but I still get only one trace shown on the analyzer which is set to clear write for some reason.

Attached is the VI to begin with, I want to add a trace based on that.

Any help is greatly appreciated!

Harry  

Attachments

Outcomes