AnsweredAssumed Answered

AW: vrf Need help developing Linearity Test.

Question asked by VRFuser on Nov 6, 2006
Or you can use ready to run VEE-programs for your purpose. Have a look in the example folders under Help menue, and look in the subfolder instrumentIO.
An even easier way is to use the iomanager, search for instruments and then load an example - lower right button...

-----Ursprüngliche Nachricht-----
Von: fukui.yutaka@jp.fujitsu.com [mailto:fukui.yutaka@jp.fujitsu.com]
Gesendet: Dienstag, 7. November 2006 02:22
An: VRF
Cc: VRF
Betreff: Re: [vrf] Need help developing Linearity Test.

Hi,
Open VEE and then click
help -> Agilent VEE on the Web -> Instrument Drivers!
You can find drivers there.
Drivers:
Agilent E4408B ESA-L Series Spectrum Analyzers, 9 kHz to 26.5 GHz
http://adn.tm.agilent.com/index.cgi?CONTENT_ID=2622
Drivers:
Agilent 8753ES S-parameter Network Analyzer
http://adn.tm.agilent.com/index.cgi?CONTENT_ID=2495
Regards,
FUKUI Yutaka
----- Original Message -----
>Subject: [vrf] Need help developing Linearity Test.
>Date: Tue, 7 Nov 2006 08:19:41 +0800
>From: "MOHD-KAMAL,MAT-ZAIN (A-Malaysia,ex1)"
><mat-zain_mohd-kamal@agilent.com
>
>To: VRF <vrf@agilent.com>
>
>
>Hi friends
>I need help. Im currently developing linearity test using vee platform.
>I hav
e difficulty in finding driver for instrument. I need to find driver for E4418 B EPM Series Power Meter and 8753 ES S-Parameter Network analyzer. Thanks
>
>Regards
>Kamal
>

---
To subscribe please send an email to: "vrf-request@lists.it.agilent.com" with the word subscribe in the message body.
To unsubscribe send a blank email to "leave-vrf@it.lists.it.agilent.com".
To send messages to this mailing list,  email "vrf@agilent.com". 
If you need help with the mailing list send a message to "owner-vrf@it.lists.it.agilent.com".
Search the "unofficial vrf archive" at "www.oswegosw.com/vrf_archive/".

Outcomes