AnsweredAssumed Answered

Calpod controller be connected to 2 PNA-X's?

Question asked by rok on Nov 8, 2013
Latest reply on Nov 19, 2013 by rok
Hello,

I'm looking at the Calpod 85523A controller which can control 4 calpods without a splitter. I was wondering if I can hook up 2 PNA-X's to talk to the same CalPod controller and have them operate in recorrection at the same time. For instance, Ports 1 & 2 of the Calpod controller is connected to calpods for PNA-X #1 and Ports 3& 4 of the calpod controller is connected to calpods for PNA-X #2 and I'm initiating the re-correction operation on both PNA-X's simultaneously. 


Thanks,
rok  

Outcomes