AnsweredAssumed Answered

N57xx series question about current programming accuracy

Question asked by zs on Oct 31, 2013
For the N5766A (1500W) there is a spec for current programming accuracy (0.1% + 38mA) and for current measurement accuracy (0.1% + 114 mA).
Is the programming dependent on the measurement accuracy?
In other words - when I program for 13A, will the accuracy be expected within 0.1% + 38 mA or within 0.1% + 38 ma + 114 mA?

The spec can be read both ways and I am asking because I have encountered an issue writing a program verifying that the unit is within spec.  

Outcomes