AnsweredAssumed Answered

millimeter wave noise figure measurement(57 to 65GHz)

Question asked by nsm on Oct 10, 2013
Latest reply on Oct 14, 2013 by david_ballo
hi,

I am interested in making noise figure measurements in the 57 to 65GHz band on an amplifier using the PNA-X.As I understand,the low noise receivers work up to 50GHz. However for the higher band, we need to use a pre amplifier with a filter. The noise figure of my device is around 5 to 10dB and the gain is around 12 dB. Can you recommend a pre amplifier and filter that I could use for this measurement?

Rgds  

Outcomes