AnsweredAssumed Answered

81635A logging results

Question asked by kobika on Mar 20, 2014
Hello
i am using vb.net and.
i am using the following test equ.: Tunable laser 81980A and power meter 81635A - both on one frame 8163B.
my target is to do sweep with the laser and record the results in the power meter.
i succeeded to do so but the only issue i have is the result feedback i get for the result command:

"SENSE2:CHAN2:FUNC:RESULT?"

what i am getting is the following string:
"#252]ע9utע9ץˆע9ץ‘ע9}Œע9ץ‘ע9uע9u§ע9°ע9°ע9u¾ע9}×ע9u§ע9\n"

does anyone have an idea how should i convert this to a real numbers ?
does anyone have the 816x dll for using in vb.net?
thanks

Outcomes