AnsweredAssumed Answered

Agilent N5230C 2 Port Analyzer De-embeding Save and Recall

Question asked by pennsy on Feb 7, 2014
Have VB6 Test Software for 5230A  that works fine for Saving and Recalling the S2P files on an exsiting test Program.  Using  Same Code for the 5230C when Recalling the S2P file that is required, I'm getting and Additional window with the measurement traces that shows up each time on the display, and also loose the Correction.   Files seem to be saved Ok on the 5230C.   Do I nned  to recall the S2P differently or maybe save the S2P differently for the 5230C ?

Edited by: pennsy on Feb 7, 2014 5:28 AM  

Outcomes