AnsweredAssumed Answered

How many samples can be digitized

Question asked by rickc Employee on Jun 6, 2013
Latest reply on Jul 22, 2013 by KiriakosGR
The Multimeter Connectivity Utility supports both datalogging and digitizing of signals. 
Digitization is supported by taking measurements and storing them into the internal memory in the DMM. The number of samples that can be digitized is limited to this internal memory.  

When using the utility, you won't see this limit listed on the screen or in the help file, but if you try to enter a value that is too large it will be reset to the maximum value allowed by your DMM. 
So for example, on my 34410A DMM, I enter a value of 50000, after I hit enter it will return with the value set to 10k.  

Outcomes