AnsweredAssumed Answered

PNA-X - How to show the smoothing value used for a trace in printout

Question asked by rok on Aug 2, 2013
Latest reply on Aug 5, 2013 by rok
Hello,

I'm using the A.09.90.01 firmware. Is there a way to see the smoothing % value (if enabled) used for a particular trace (from any measurement class) in the printout, much like how the 'Avg' is implemented? (i.e. shown in the lower left hand corner of the screen) Or even put it in the trace attributes table that is on the second sheet of the printout? I looked in the 'Page Setup' section, but it didn't have any option for it. 

Thanks,
rok  

Outcomes