Hi,
I am having an error on simulating a component modeled and simulated in the layout and inserted back into the schematic for ADS 2011.10. I get an error regarding the pins not corresponding to each other from the layout to the schematics. I have followed the outlined instructions for inserting components from ADS docs but still have yet to find a solution. The following pics outline the issues:
http://imgur.com/a/JeCOo
Thank you.
I am having an error on simulating a component modeled and simulated in the layout and inserted back into the schematic for ADS 2011.10. I get an error regarding the pins not corresponding to each other from the layout to the schematics. I have followed the outlined instructions for inserting components from ADS docs but still have yet to find a solution. The following pics outline the issues:
http://imgur.com/a/JeCOo
Thank you.
I tried changing the settings for the model settings and I still get the same error. I played with it quite a bit and still no luck. Here's the error messages and design settings I used for simulation:
http://imgur.com/k1QNFxI
Looks like the simulation doesn;t recognize the two placed pins inside the layout window? (error says 2 pins and 0 pins in schematic & layout)
Any ideas?