AnsweredAssumed Answered

Do the pins for the handles fall out of FieldFoxs??

Question asked by drkirkby on Apr 16, 2014
Latest reply on Apr 18, 2014 by drkirkby
On this eBay auction

http://m.ebay.co.uk/itm/380882768891

there is an N9912A. The two stainless steel pins which are used to fix the handle on the top can be seen missing in the third photo. I bought that instrument,  and although it is not shown,  one of the pins is missing on the side too. So 3 of the 4 are missing.  

I have seen another N9912A which suffered the same fate. No damage can be seen to the case, so I can't understand how the pins are not present. 

Is this a common fault? It is a bit worrying if the supports for the handles fall out. 

I gather from someone else whose FieldFox suffered the same problem that it wss cheap to buy the pins. But I am reluctant to ever used the handles if they break offf for good reason. 

Dave.  

Outcomes