AnsweredAssumed Answered

X-parameter application note

Question asked by DSTEPHENS on Jun 18, 2014
Latest reply on Jun 18, 2014 by daras
Hi there,

I would like to ask if you have an application note illustrating the setup for performing a 2-tone X-parameter characterization (IMD analysis). The PNA-X I have has two signal sources and is capable of performing single tone X-parameter measurements (though I am yet to set this up). Looking ahead, my real goal is to have a X-parameter model that can be used for IMD analysis and as such I would like to know what additional equipment is needed. I am hoping that only one additional signal source is required and that the characterization tone from the PNA-X will be sufficient for a 2-tone characterization.

Many thanks for your time.

Daniel  

Outcomes