AnsweredAssumed Answered

ENA Ports Close Together

Question asked by opticyclic on May 15, 2006
Latest reply on May 24, 2006 by mmule54
Why are the ENA ports so close together?
Why are the 4 ports not spaced equally along the bottom of the analyser?

This is fundamentally a bad design.

I tried to measure in 14 mm and 7-16, but I physically can't connect 2 adaptors next to each other in the current configuration.

I know I could use port 1 and port 4 for example, but what about 4-port measurements (in a smaller line size)?
It becomes very difficult to do the adaptors up even then.  

Outcomes