AnsweredAssumed Answered

PNA-X pdf page number problem

Question asked by rok on May 15, 2014
Hello,

I am using A.09.90.09 firmware on the PNA-X. I am trying to create a PDF with page numbers enabled. The problem I am running into is that sometimes, it would print extra page numbers that doesn't make sense, in addition to the correct page numbers when I am printing to the 'PDF995' printer that is provided on the PNA-X. I have attached a sample. The problem is intermittent, so sometimes it works and sometimes it doesn't. If someone can investigate to figure out why this is happening, that would be greatly appreciated.

Thanks,
rok  

Outcomes